Part Number: TLC27L4B Dear
I am writing to you regarding the component in question, part number TLC27L4BIDR, to bring to your attention a serious technical issue that is impacting the production of one of our
We look forward to your prompt response…
Part Number: OPA2991 We are designing a 6-channel active analog output board using OPA2991IDR.
Application summary:
Supply to OPA2991IDR: 12 V single supply
DAC input signal: 0 to 2.5 V
Op amp configuration: non-inverting gain stage…
Hello SAKTHIRAAM,
The LMH6554 is a fully-differential amplifier which will work for this application with the ADC12DL2500. There are some considerations which need to be made:
- The ADC12DL2500 has an input common mode of zero volts, so there is not…
Part Number: CC1310 Tool/software: We have been using Qualcomm SAW filter (Part Number: B39871B3717U410) which incorporates the TI CC1310 chipset.
Issue Summary:
The affected product was assembled and tested successfully in February 2021 and subsequently…
Part Number: OPA858 Other Parts Discussed in Thread: THS4541 , OPA859 Hi Team,
1. Should the Vref of OPA858IDSGR be connected to a 2.5V bias voltage or to ground? If OPA858 is used as a transimpedance amplifier (TIA), is the output voltage formula:…
Part Number: CC2755R10 Other Parts Discussed in Thread: LP-EM-CC2745R10-Q1 Tool/software: Hi,
I would like to get LP-EM-CC2745R10-Q1 RF test report, including:
(1) RSSI vs range (RVR)
(2) Receiver sensitivity data
Hi Rob-san,
Thank you for your support.
How is the progress on this matter?
The device’s thermal resistance is specified in the datasheet, but when estimating from the surface temperature, the thermal resistance between the junction and the device…
Part Number: CC2652R Other Parts Discussed in Thread: CC2592 , Dear All,
In my project for range extenstion I am using cc2592 with cc2652r. only 2 meters range getting. attaching the configurations .
#include <ti/drivers/rf/RF.h>
// void rfDriverCallbackAntennaSwitching…
Hi Colin,
Colin Chen said: Can this be provided? No specific quantity is required, only a range is needed, such as within 50?
Both OPA4991-Q1 and LM2902BA-Q1 are quad op amp. The total transistors in each op amp is more than 50 (each op amp number…