Part Number: MMWCAS-DSP-EVM Hello Experts, Please let us know the operating temperature range (Ta) of MMWCAS-RF-EVM and MMWCAS-DSP-EVM. We are seeing an issue when the ambient temperature is 10~15 degree C. Best regards, Ken
Part Number: AWR1243 Whether this device will support triangular chirp signal. Since triangular chirp signal can estimate range and doppler in one chirp itself, Why these devices use series of saw tooth chirps for estimating the velocity/doppler.
1…
Hi Hemil,
Range is dependent on multiple variables and it is not straightforward to calculate distance vs transmit power. the PHY used, antenna type, height and placement, as well as the environment and noise affect range.
As a rule of thumb for every…
Part Number: CC1110-CC1111 For different radio chips we use the Excel-sheet, mentioned under Thread title, to calculate and judge different radios, modulation formats, output power etc.
When using version 1.17 a new parameter has shown up. This is under…
Part Number: MMWCAS-RF-EVM
Hi,
I am currently working with mmwave studio version 3 and when I run the mmwave_studio_03_00_00_07\mmWaveStudio\MatlabExamples\4chip_cascade_MIMO_example\main\cascade\input\cascade_MIMO_signalProcessing.m file, I get the…
Part Number: CC1310 Hi All,
We designed and developed a project using CC1310. In this project, we built custom boards as per the CC1310 with help from Application Report SWRA524A. The boards are 4-layer impedance controlled boards. Pictures of schematics…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: TDA2 , AWR2243
Hi,
I am using AWR2243 MMWCAS-RF-EVM/MMWCAS-DSP-EVM with processor sdk for radar v3.8. I put one corner reflector in boresight of the cascaded EVM and ran the default TXBF…
Hi,
Most of this can be found in the datasheet ( CC1352P Datasheet: https://www.ti.com/lit/swrs192 ):
The characterised CC1352P7 Wi-SUN PHYs are all 2-GFSK.
RX performance: There is a sub-section for Wi-SUN PHYs in Section 8.10
Power consumption…
Part Number: CC1310 Hello,
is it possible to export the plotted data out of the range estimation spreadsheet? I would like to plot the data myself in an different context.
Thank you
Part Number: IWR6843 Hello TI,
I would like to ask what is the proper way of interbin resolution calculation. Taking "Short Range Default" configuration in Sensing Estimator I got something like:
Range interbin res. = 4.36cm
Velocity interbin…