Part Number: RF430FRL152HEVM Other Parts Discussed in Thread: TRF7970A , RF430FRL152H , RF430FRL153H , RF430FRL154H Hi team,
i am trying to send NDEF message from RF430FRL152HEVM to trf7970a,
i got the sample example where it consists of single NDEF Message…
Hi Fengzhou,
depending on what your application is, you may have a look to the following devices:
RF430CL330H ( https://www.ti.com/product/RF430CL330H ), which can provide data as NDEF message. This device needs in addition a MCU but a complete passive…
Part Number: RF430FRL153H Other Parts Discussed in Thread: RF430FRL152H , RF430FRL154H , RF430FRL152HEVM , DLP-7970ABP , TRF7970A , MSP-FET , PCA9306
Hello,
I intend to use the RF430FRL153H for a project. I need to read an analog sensor and, after the reading…
Hello Vamsi,
1. No, the TRF7970A cannot emulate an ISO15693 tag. Card emulation (CE Mode) is only available for ISO14443A/B.
2. Same reason as 1. The TRF7970A cannot answer ISO15693 requests.
3. This is possible with the RF430FRL152H. Its primary usage…
Part Number: RF430FRL152H Other Parts Discussed in Thread: RF430FRL154H , BQ25570
Dear TI,
Currently, I have been conducting research for my thesis project that is supposed to be COMPLETELY POWERED by RF WAVES (in short, it is a battery-less powered circuit…
Hello Helfried,
I show you the defines:
#define CLEAR_BLOCK_LOCKS BIT3
#define FRAM_LOCK_BLOCK_AREA_SIZE 38
#define FRAM_LOCK_BLOCKS 0xF840 //Address of ISO15693 lock…
Yes leaving them unconnected should be fine.
Also I would recommend that if you are not using the SD14 at all, consider using RF430FRL154H since it will be cheaper for your application.
Hi Alex,
I have more questions about your answer.
1. Regarding the NFC task functions, you don't have a plan to update the RF430FRL154H in the future?
2. I'm planning to use the RF430FRL154H for my mass production. But the RF430FRL154H sample is not…