Hi Yohei,
The internal cavity of SE555-SP in CDIP is 21.471 mm^3 or 0.02147 cm^3. I believe that this is excluding SE555's die and bonding adhesives.
I do not have figures in actual internal volume of the SE555-SP part.
If you have additional questions…
Part Number: SE555 Other Parts Discussed in Thread: TLC555M Can you suggest any alternate part number for this part number SE555D with similar functionality which will work in ambient temperature range of -46 deg Celc to 136 deg Celc and Max Junction…
Part Number: SA555 Other Parts Discussed in Thread: SE555 , , NE555 , NA555 Hi team,
Could you tell what makes NA555, NE555, SE555 and SA555's operating tempreraure ranges different?
NA555, NE555, SE555 and SA555 look similar but customer wants to …
Part Number: SE555 Other Parts Discussed in Thread: TLC555-Q1 Hi team,
SE555 product page says it is an automotive grade part, however in datasheet there's no description on this.
Could you please help confirm?
Thanks,
Scarlett
Part Number: SE555 Other Parts Discussed in Thread: SN74AHCT00Q-Q1 ,
Hello,
This might be an FMEA-related question, but does the SE555DR have a failure mode that causes its OUT pin (pin 3) to stick to High?
Best regards, Shinichi Yokota
Part Number: SE555 Can any one provide SE555DR's
ESD (HBM MM CDM)HBM---HUMAN BODY MODE--- 2KV MINIMUM MM ---MACHINE MODE---200V MINIMUM CDM — CHARGE DEVICE MODE---1KV MINIMUM
Part Number: SE555 Hi E2E
I am using SE555 in Astable operation for generating a PWM signal of ~38kHz.I have chosen the resistors R A R B and capacitor C as per the formula given in the datasheet under 8.3.2 A-stable Operation.
Attaching that datasheet formula…
Part Number: SE555
Hello,
I've noticed SE555's sequential timer circuit in Figure 22 of its data sheet violates its TRIG pin's absolute Max rating. Do you agree with me? The TRIG pin's absolute Max rating is defined as V CC (Max), but…