Part Number: SE555-SP Other Parts Discussed in Thread: TLV4H390-SEP Tool/software: Hello, I am designing a radiation-hardened circuit that needs to latch an output state for a relatively long time duration of 100ms after a change in the input state. After…
Part Number: SE555-SP Other Parts Discussed in Thread: SE555 , TLC555 Hi
I need to know max freq of operation of the SE555-SP part and if there is a PSPICE model available?
Thanks
Part Number: SE555-SP The SE555-SP datasheet shows that the device has trigger and threshold voltage characterized at several supply voltages and temperatures, but there is no information on what is driving these variations. If possible, I would like…
Hi Yohei,
The internal cavity of SE555-SP in CDIP is 21.471 mm^3 or 0.02147 cm^3. I believe that this is excluding SE555's die and bonding adhesives.
I do not have figures in actual internal volume of the SE555-SP part.
If you have additional questions…
Part Number: SE555-SP Other Parts Discussed in Thread: SE555 Hello,
I would like to know if the SE555-SP is subject to SET in radiated environement ? We look into the radiation report but we find only TID datas.
I have the same question for the SE555…
Part Number: TL1431-SP Other Parts Discussed in Thread: SE555-SP , TMUX182-SEP , TPS7H5020-SEP , TLV1704-SEP , TPS7H4010-SEP , INA950-SEP , TPS7A4501-SP , ISOS141-SEP , LM158QML-SP , DS26F32MQML-SP Dear TI Support Team,
We are reviewing several TI space…
Other Parts Discussed in Thread: SE555-SP , NE555 , TPL5010 , TPL5110 , BQ32000 , BQ32002 Hi, everyone.
I am running a project in which I need a very precise square wave generated with the use of 1 external Capacitor. I know that NE555 would make the…
Hi Ron,
That is good information!
What are the differences between the M38510 and the SE555xxB devices? Are they adhering to different military standards? Is there a datasheet available there?
I am trying to get a quote for the SE555-SP device but…