Part Number: LAUNCHXL-CC1352P Other Parts Discussed in Thread: BOOSTXL-SHARP128 , SIMPLELINK-CC13X2-26X2-SDK , SYSCONFIG Hello,
I own an evaluation board LAUNCHXL-CC1352P-2.
I am developing a small Zigbee application. I also have a BOOSTXL-SHARP128…
Part Number: SIMPLELINK-CC13X2-26X2-SDK Other Parts Discussed in Thread: CC1352R Tool/software: Hi,
I am currently reviewing the Bluetooth Core 5.2 qualification tests for CC1352R in the bluetooth qualification workspace.
https://qualification.bluetooth…
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK Other Parts Discussed in Thread: CC1352P Tool/software: Hi.
I want to create the project which is rxAudioTx example at launchpad CC1352P.
When I create the example, I got the error message below:
Project…
Part Number: SIMPLELINK-LOWPOWER-SDK Tool/software: Hi,
Which version of Bluetooth specification does the bluetooth stack in simpleLink SDK(latest 8.40) con forms to?5.2, 5.3 or 5.4?Target chip is CC2745P10. Thanks.
Part Number: SIMPLELINK-SDK-BLUETOOTH-PLUGIN Other Parts Discussed in Thread: MSP432E401Y Hello.
Does SIMPLELINK-SDK-BLUETOOTH-PLUGIN supports MSP432E401Y?
How should I implement BLE to MSP432E401Y regarding software?
Regards,
U-SK
Part Number: SIMPLELINK-LOWPOWER-F3-SDK Hello TI Team,
<Usage Conditions>
SIMPLELINK-LOWPOWER-F3-SDK: v9.20.00.81
IAR Embedded Workbench: v9.70.2 (Japanese Version) *
This is the version listed in the release notes.
<Description> When…
Part Number: SIMPLELINK-MSP432-SDK
Tool/software:
Hi,
I am using MSP432P401R with FreeRTOS.
For most work, I need to use the SDK and driverlib. It works fine when I use example projects from the SDK.
But when I use FreeRTOS example projects…
Part Number: CC1312R (1)During audio testing using the CC1312R audio plugin SDK, I observed glitches in the output analog signal. Where could these glitches be coming from, and how can I fix them? I'm using the development kit recommended for the audio…
Part Number: MSP432P401R Other Parts Discussed in Thread: ENERGYTRACE Hello,
I have confusion regarding SimpleLink SDK Bluetooth Plugin with MSP432P401R + CC2640R2. It says that to achieve deeper low power mode such as LPM3, the SAP_close must be called…
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK Other Parts Discussed in Thread: SYSCONFIG Hello,
My customer uses CC2642 and recently moved from SDK v6.10 with IAR v8.50.5 to SDK v6.30 with IAR v8.50.9. Now the TI-RTOS plugin doesn't work anymore in IAR…