Part Number: SMV512K32-SP Hi All,
Can you please provide me some space grade memory parts - SRAM, DDR3, FPGA PROM ?
NOR FLASH : 256MB DDR3 : 1 GBYTE
Thanks
Part Number: SMV512K32-SP Other Parts Discussed in Thread: SMV512K32 The SMV512K32 datasheet specifies that the 3.3V VDD2 current draw when reading at 50 MHz is 275 mA up to 25C, but only 120 mA at 125C. What is the expected VDD2 current draw for temperatures…
Other Parts Discussed in Thread: SMV512K32-SP For hardware testing purposes, is there a way to cause the SMV512K32-SP to generate an MBE for a particular address?
For example: If I disable EDAC, write to a location, then enable EDAC and read that location…
Table 2 in the datasheet shows an "Example Control Setting for Resetting MBE". The term "example" suggests that other alternatives are possible.
First, the table shows both E1Z and E2 being deasserted. The text suggests that E1Z could…
When a read operation occurs with a single-bit error and the corrected data is presented to the output, is that corrected data immediately written back to the memory array to correct the storage cells or does the part rely on the scrubber to correct the…
Other Parts Discussed in Thread: SMV512K32-SP Could you explain about Scrubing Function as SMV512K32-SP SRAM.
What does it operate ? What is Scrubing ? What is diffrenct form EDAC?
Thank you.
Mtisu
Hi Tilman,
Welcome to E2E Design Support Community!
We are actually working on updating our TI Space Products Guide (ti.com/spaceguide) to include a list of Dummy Packages / Mechanical Samples, which should be updated in the coming months. In the meantime…