Part Number: SN65HVD230 Other Parts Discussed in Thread: TCAN1057A-Q1 Tool/software: Hi,
I am evaluating to change the CAN driver for the SN65HVD1050DR.
Both part numbers are pin to pin compatible but the voltage range is different.
For the SN65HVD230 …
Part Number: SN65HVD230 Tool/software: Hello,
there are two common types of termination - standard and split. Some questions arise around implementation. 1) When multiple nodes are on the same bus, one 120 Ohm resistor must be at the start and another…
Part Number: SN65HVD230 Tool/software: I have been using SN65HVD230DG4, but I was recommended to use SN65HVD230DR because of ESG support.
In order to switch to the part with the suffix of DR, please tell me the following contents.
①Is the plating material…
Part Number: SN65HVD230 Other Parts Discussed in Thread: ESD2CAN24-Q1 , ESD2CAN36-Q1 Tool/software: Using the SN65HVD230DR CAN transceiver with an MCP2515 CAN controller.
This is successful past circuit being used in a new application.
Running both chips…
Hi Shubham,
Shubham Goel said: Can you please confirm if Pinmux_init is mandatory to integrate for user expansion connector
Yes pinmux is necessary. It might work in some cases, as the pins by default are set to work as CAN, but this might or might not apply…
Part Number: SN65HVD230 Tool/software: Hi team, I'm considering to using the TCAN1044. I found the application note(SLLA270) for Stub Length. Can bellow comment in application note still be used? >To minimized reflections, stub-line length should not…
Part Number: SN65HVD230 Other Parts Discussed in Thread: TCAN3413 , TCAN3403-Q1 , TCAN3404-Q1 , TCAN3414 Tool/software: Dear Experts,
I would like to know if +3.3V CAN can operate correctly with +5.0V CAN network seamlessly up to 1Mbit/s with also 10ms…