Other Parts Discussed in Thread: TMS320F28035 , SN65HVD230 , SN65HVD231 , SN65HVD232 While doing the CAN communication between TMS320F28035 and Arduino or Peak CAN analyzer at
1 Mbps, the data transfer was happening for all data’s and all CAN Ids in standard…
Hi Hareesh Sir,
Following are the answers to questions asked by you:-
Ans 1) Yes i am using on chip zero pin oscillator(Internal Oscillator 1). So firstly when i implemented CAN application code for TMS320f28035 i didn't include any code for calibration…
While doing the CAN communication between TMS320F28035 and Arduino or Peak CAN analyzer at
1 Mbps, the data transfer was happening for all data’s and all CAN Ids in standard mode.
But once the Baud rate was changed to 500Kbps, the data transfer…
Hi Dhruve,
I think you will find with a slightly tighter supply voltage (3.3V ±10%) you will find that you have much more transceiver options available to you. Here are the 3.3 volt transceivers that we have in our portfolio.
SN65HVD235 -…
Other Parts Discussed in Thread: SN65HVD231 Hello,
where can I find examples for the usage of CAN mode, but not just in self test as the back2back example from the example list.
For Infomation:
I use the transceiver: sn65hvd231
And a CAN Bus with one device…
Hi Livio,
TI has several 3.3V CAN transeivers (Automotive and Catalog). You can use either of them for your application. SN65HVD230, SN65HVD231, SN65HVD232
For 5V CAN tranceiver, SH65HVD256 supports both 3.3V and 5V for RDX (pin 5 will not act as fault…
Other Parts Discussed in Thread: SN65HVD231 , ISO1050 I am no expert on CAN, but would like to know whether it is possible to have (say) 200 to 300 device nodes on a single CAN bus. I have seen on data sheet of eg SN65HVD231 that 120 nodes can be supported…
Hi Govind,
Unfortunately, none of the 3.3V CAN transceivers in our portfolio have an EVM specifically made for them.
With that being said the SN65HVD257 EVM that you mentioned can easily be used for 3.3V CAN transceivers, but I think the SN65HVD255EVM…
Other Parts Discussed in Thread: SN65HVD232 , SN65HVD231 In case of IC SN65HVD231, CAN communication breaks
down or error frames generate as motor starts. In normal conditions when motor
is not operational, CAN communication occur nomally. If we replace…
Other Parts Discussed in Thread: SN65HVD230 , SN65HVD257 , SN65HVD231 I have read the datasheets for these parts, and I understand that the signaling is compatible with "standard" 5V CAN transceivers. But the datasheets don't mention how the transceiver…