Part Number: SN65HVD231Q
The above circuit is located into two places. One is in a cockpit of an aircraft as a controller with this CAN interface; the other is on a transmitter located about 30 feet past noisy generators and the like. We brought the…
Part Number: SN65HVD231 Dear team,
May I double confirm below item with you? Thanks.
Does our SN65HVD231D & SN65HVD231Q-Q1 can both compatible with ISO11898(1-5) and ISO16845?
Ben
Part Number: SN65HVD231Q-Q1 Other Parts Discussed in Thread: SN65HVD231 , Hi,
I need Junction to Case Thermal Resistance (Rjc) and Junction to board Thermal Resistance (Rjb) details for SN65HVD231QDRG4Q1 component. Also, junction temperature limit. It appears…
Other Parts Discussed in Thread: SN65HVD231Q , SN65HVD255 Dear TI Engineer,
Can I get SN65HVD231Q EVM documents? or its reference schematic?
Because I've found only the Datasheet on TI website!
Otherwise, Could you review this schematic?
It's for BMS CAN…
Sorry, my mistake on the question.
The parts I am looking at include the SN65HVD230Q-Q1 and the SN65HVD231Q-Q1 (I was not aware of the very similar part you were referencing in your answer).
However, the absolute maximum table is not clear about the conditions…
Hello,
Please take a look at SN65HVD231Q. It is a very similar device that is specified to support ambient operating temperatures up to 125 C.
Regards, Max
Hello Kay,
SN65HVD231Q requires that the bus signals operate in a -2 V to +7 V range. Normally CAN bus signals will be within this range, although if shifts in ground potential are present between nodes the bus voltage range can increase. If the application…
Other Parts Discussed in Thread: SN65HVD232Q , SN65HVD231Q , SN65HVD230Q Hi,
I am looking at using the SN65HVD232Q with a Microchip can controller as I am making a small revision to an existing product and I want to use a 3v3 CANbus transceiver with automotive…
Hello Luxi,
Yes, you would need a CAN Trasnceiver. About a month back we ran a lot of CAN posts, one of which had the CAN Transceiver mentioned. I would suggest SN65HVD231Q
Regards
Amit