Part Number: SN65HVD256 Other Parts Discussed in Thread: SN65HVD234-Q1 , TCAN332 , TCAN1051 hi,
I want to know ,if i use the sn65hvd256 in 3.3v system, could i connect the Vcc and Vrxd all to 3.3v power supply? or do i need connect two power supply rail…
Part Number: TMS570LS0432 Other Parts Discussed in Thread: SN65HVD234
Hello.
I am building a custom board for TMS570LS0432 micro-controller and have a doubt regarding the transceiver hardware for the CAN pins. According to the launchpad schematics, there…
Hi Richard, I missed that it has to be a 3V3 device. I have put together a comparison with 3V3 devices here ->
http://www.ti.com/assets/js/compareParts/compare.html?familyId=540&parts=TCAN330,TCAN332,TCAN334,TCAN337,SN65HVD232Q,SN65HVD234-Q1,SN65HVD1040…
Unfortunately, this device could be damaged by any voltages on the CAN pins exceeding +/- 14 V, as indicated by the "absolute maximum" ratings table in the datasheet. To pass this test, you could design a circuit which disconnects the transceiver from…
Todd,
Thanks for your message.
You're right, I found this link where I could compare different LaunchPads:
It seems "LAUNCHXL-F28069M" fits my need as it comes with "SN65HVD234" CAN transceiver.
Thanks,
--Kash
Other Parts Discussed in Thread: MAX3232E-Q1 , SN65HVD234 Hi Team, May I have "Equivalent Input and Output Schematic Diagrams" for MAX3232E-Q1? The datasheet (page 18) of SN65HVD234 shows the following and my customer wants same information for…
Part Number: SN65HVD1781 Other Parts Discussed in Thread: SN65HVD234
Does the +-70V fault protection on the SN65HVD1781 also include protection against putting 70V directly across the A and B terminals? From what I can tell from the datasheet it looks…
Part Number: TMS320F28069M Other Parts Discussed in Thread: CONTROLSUITE , HALCOGEN , SN65HVD234 , ISO1050
Hello,
I am using LAUNCHXL28069M KIT along with my development board having TMS570LS4x micro controller for CANBus communication.
LAUNCHXL28069M as…
Hi Andrew,
The above launchpad does have a CAN Transceiver SN65HVD234D
You can download the datasheet from this link: www.ti.com/.../sn65hvd234
Regards,
Gautam