Part Number: TPS4HC120-Q1 Hello TI Team,
I have a few questions regarding the TPS4HC120-Q1.
Operation with VBB = 5 V
According to the datasheet, the nominal operating voltage range for the VBB pin is 4 V to 18 V. However, many of the electrical…
Part Number: TDA4VH-Q1 Could you confirm if there are any internal hardware differences between the General purpose part (TDA4VH88TGAALYRQ1) and High security, R5F lockstep capable part (TDA4VH88T5AALYRQ1), or are these using the same silicon?
Part Number: TPS1HTC30-Q1 Hi,
I am using the TPS1HTC30AQPWPRQ1 and found a contradiction in the datasheet (SLVSGL4A, revised May 2026) regarding the EN pin.
(a) Table 5-1. Pin Functions, EN pin: "Enables/disables channel output current, internal pullup…
Part Number: TPS546D24A Other Parts Discussed in Thread: TPS543C20 , LMQ644A2-Q1 , LM3880 , TPS386000 , TPSM5D1806 Hello TI Team,
I am designing a power supply and sequencing solution for an Intel/Altera Agilex 5 SoC and would like to verify the suitability…
Part Number: TCAN1042-Q1 Hello team,
My customer mistakenly pull up the pin 5 in the Gerber, which should be NC, is there any influence? Is it necessary to change it?
BR,
Daniel
Part Number: TDA4AL-Q1 Hi TI Expert :
I have TDA4AL-Q1 MIPI CSI RX appliction question as blow list ,Pls help to clarify
Questions:
Does the TDA4AL CSI RX hardware support decoding up to 5 Data Types simultaneously in a single stream?
…
Part Number: LM706A0-Q1 Other Parts Discussed in Thread: LM706A0 Tool/software: Hi all,
I use LM706A0 EVM board to test 48Vin/3.3Vout@max 10A condition and see the transient regulation out of 5%.
Transient condition is 4A to 10A with 2.5A/us, using…
Part Number: TCAN2845-Q1 Tool/software: Hi,
One of my customer is considering TCAN28473/5 for automotive design. We are planning to use this regulator supply 3.3V to an off-board sensor, and it is essential that this supply is protected against both…