Hi Team,
My customer would like to connect the SWAP pin to VDD=1.8V.
In this case, must they connect the pull up resistor?
If yes, Could you please let us know the recommended value?
Regards,
Kanemaru
Other Parts Discussed in Thread: SN65LVDS301 , SN65LVDS302 Hi Team,
Our customer is simulating SN65LVDS301/302 using IBIS model.
The simulation result of SN65LVDS302 input voltage was +/- 400mV.
It seems there is no 100 Ohm termination resistor on the input…
Hello Kum,
I am out for a business travel, so I 've been unable to address the query. However you have nothing to worry, these devices have been tested toghether. In fact you can compare the SN65LVDS314 (Datasheet, page 14) with the SN65LVDS302 (darasheet…
Hi Michael,
Thank you very much for your reply and suggestion. I have not gone through the specs of SN65LVDS302 in details but it seems that its speed is insufficient for us.
The block diagram looks like this:
The clock runs in GHz range (depending on…
Other Parts Discussed in Thread: SN65LVDS301 , SN65LVDS302 Hi, is there a simulation model (SPICE or IBIS model) for SN65LVDS301 and SN65LVDS302 ?
I couldn't find them on the WEB.
We are requested from our customer for simulation.
Best Regards,
Ka…
Hello,
I can suggest you useful information about hardware schematic, software settings and interfacing to the LVDS display from the DM3730 side by looking at the section 15.6.4 How to Interface OMAP Device With SN65LVDS302 Receiver for an XGA Display…
Other Parts Discussed in Thread: AM3505 , SN65LVDS302 Hello,
My customer wants to use SDI interface from AM3505 in order to reduce number of signals going to LCD.
However, LCD has 28bit parallel interface. The customer is thinking of using SN65LVDS302…