Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: SN74LS125A , SN74AHC1G125 On parts like the Quad Bus Buffer SN74125 (not the SN74LS125A) there is a Short Circuit Output Current (Ios) parameter that states the output current when a gate being shorted. On the SN74125 a…
Other Parts Discussed in Thread: SN74AHCT1G125 , SN74AHC1G125 , SN74LVC1G97 Hi all Would you mind if we ask SN74AHC1G125 and SN74AHCT1G125? Do these devices have spec about Vh(Hysteresis voltage)? We could not find it on the datasheet. So, could you let us…
Part Number: SN65HVD1040 Other Parts Discussed in Thread: TCAN334 , SN74AHC1G125 , TMS320F28377D Is RXD/TXD pin supporting 3.3V level from MCU like as F28377?
Regards
Brian
Other Parts Discussed in Thread: SN74AHC1G125 Hi
SN74AHC1G125 has overshooting and undershooting over absolute voltage.
(see attached file : overshoot is 0.8V(>0.5V), undershoot is -1.08V(<-0.5V))
Now I check how to mearure,.
However if this wave…
Other Parts Discussed in Thread: SN74LVC1G125 , SN74AHC1G125 , DS90LV012A , DS90LV011A , DS90LT012A , THVD1450 Hi Team,
Can you please help us with our customer's inquiry below.
I am looking to create a TTL transmit and receive circuit using single ended…
This will work. The electrical characteristics are guaranteed as long as you stay inside the recommended operating conditions.
For downtranslation, you can also use any buffer with overvoltage-tolerant input, i.e., SN74AHC1G125/126, SN74LVC1G34/17/125…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74AHC1G125 , SN74AUP1G125 Dear Team,
Could you share the difference between SN74LVC1G125/SN74AHC1G125/ SN74AUP1G125 ?
More further question is that what's the difference between different technology…
The only difference between '125 and '126 is the polarity of the /OE or OE input. This is shown in the functional block diagram, and in the device functional modes table.
If you want an alternative for the SN74LVC1G125, use the SN74AHC1G125 (lower…
There are no buffers that tolerate 12 V at their output. If the buffer gets damaged and creates a short from the output to VCC, then all other devices connected to VCC might see 12 V.
Anyway, you can use any 5 V buffer, such as the SN74AHC1G125 or SN74LVC1G125…
Buffers and translators have a different pinout.
Possible alternatives are SN74AUP1G17, SN74AHC1G125, or SN74LVC1G17, depending on what drive strength you need.