Ok let me explain what i want exactly :
My main goal is to generate a 1 pulse per second using a duty cycle of 50% by a 12.8MHz external oscillator.
I already have a printed PCB for that project which means i got to understand what the previous designer…
VT- max and VT+ min can over lap. The Hysteresis is still guarranteed. If the VT-max is on the upper end then the VT plus will be at least the VT- plus the hysteresis min.
The important values are VT-min and VT+ max. These are your Vil and Hih levels…
Hi Eknath ,
Schmitt trigger devices are recommended for slow rising inputs and SN74AUP1G14 is Schmitt trigger as well. It should be suitable for inputs from RC network circuits .The only thing to watch out for ,since there is slow rising inputs is the…
Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
Auto-Bidirectional Level-Shifters
Fixed DIR / DIR…