Part Number: SN74AUP1T34-Q1 Hello Team,
I had a datasheet question pop up. We are using the SN74AUP1T34-Q1 voltage level translator, and I’m trying to understand the VOH and VOL levels from section 6.3. Specifically where there might be concern is the…
Part Number: SN74AUP1T34-Q1 The Features section on page 1 says the maximum tPD at 3.3V is 3.7ns.
We have some parts in stock that are simply labelled "U4J" on the part. They were in the bin for the SN74AUP1T34QDCKRQ1.
The datasheet for that part…
Part Number: SN74AUP1T34-Q1 Logic team,
Our customer is using SN74AUP1T34-Q1 for a 100 MHz signal over -40 to +85C. Vin is 3.3V, Vout is 1.8V. It's working fine in the lab, but they want to know if this is within the acceptable range of operation for…
Part Number: SN74AUP1T34-Q1 Hi,
Could you please share the jitter performance for SN74AUP1T34-Q1 with me if you have this information ?
Best regards, Liu Xingqiao
Part Number: SN74AUP1T34-Q1 Other Parts Discussed in Thread: 2N7001T , SN74AXC1T45 in datasheet, there is only introduction about the application of signal from low voltage to high voltage. please tell if it support the voltage reduction case.
Part Number: SN74AUP1T34-Q1 Hi team.
The customer requests data about the status of the output when the input is floating.
for example, if A is floating when input status, how is B status ?
Customers want products that are equally floating.
…
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74LVC1T45-Q1 , SN74AUP1T34-Q1 , SN74AHCT1G125-Q1 Hi team,
Do we have auto grade version for SN74LV1T34?
By the way, could we use sn74lvc1t45-q1 to replace it?
Thanks.
At 20 MHz, the signal edges are 50 ns apart. The TLV3201-Q1 has a propagation delay of up to 50 ns.
The TLV3201-Q1 does not run at 1.8 V, but no fast comparator does. You need a separate buffer to shift the comparator's output down to 1.8 V, e.g.,…
Other Parts Discussed in Thread: SN74AUP1T34-Q1 , LSF0101 I has considered to design a OSCIN Voltage Translator with LSF0101 or SN74AUP1T34-Q1. Because of the circuit with resistor voltage divider has some non-monotonic signal state. so I want to know…