Part Number: SN74AUP2G17 Hello,
I am using the SN74AUP2G17 at the input of a digital circuit. I would like to know what is the required value of a pull down resistor so that the output doesn't float?
Thank you.
Part Number: SN74AUP2G17 Other Parts Discussed in Thread: SN74AUP1G17 Hello,
I would like to verify that the maximum current draw from this device over the full temperature range is 0.9 uA for *both* buffers combined. The reason I ask is because the single…
Part Number: SN74AUP2G17 Hello,
The datasheet for this device does not provide the typical current consumption at 25C and 85C. I am interested in these values. Furthermore, I am very interested in obtaining data that shows the probability that a device…
Part Number: SN74AUP2G17 Hello,
I am interested in using the mentioned buffer above in my application.
I went through the DS and could not find jitter measurements.
I would like to receive information about Jitter tests conducted on this devices.
The…
Part Number: SN74AUP2G17 Dear Team,
we are look for the input range of SN74AUP2G17DRYA?
Can the input over the supply? like 1.8V supply and with 2.5V input?
Thanks.
Shen Jun
Please note that RS-232 is an electrical standard with voltages up to ±15 V; the ESP32 does not support this.
The purpose of RS-232 transceivers like the MAX3221 or RS-485 transceivers like the SN65HVD72 is to convert between different electrical…
Part Number: SN74AUC2G04 Other Parts Discussed in Thread: SN74AUP2G17 , SN74LVC2G34 , SN74LVC2G04 Hi,
I am using 2 Pin Bicolor LED where reversing polarity change its color.
Supply Voltage :3.3V
LED Specifications are
Forward Voltage: 2V
Max Current: 2…
The datasheet specifies the Δt/Δv limit as 5 ns/V. That signal is slower.
The SN74AXC2T45 could tolerate 10 ns/V (or 100 ns/V if only one input is switching). But for slower signals, you need a device with Schmitt-trigger inputs, e.g., SN74LVC2G17…