Part Number: SN74AVC2T245 Other Parts Discussed in Thread: SN74AVC2T45 Hi,
May I know what are the differences between SN74AVC2T245 and SN74AVC2T45?
Thanks,
Philip
Part Number: SN74AVC2T45 dear :
could your help to explain why this device SN74AVC2T45DCUR have two different Device making DT2R & t2dz, and what do these two silk screens means? Thanks
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: SN74AVC2T45 I looking for low Icc(ICCA + ICCB) level shift IC.
Please let me confirm about test condition for SN74LVC2T45 and SN74AVC2T45.
Electrical characteristics are described that ICCA + ICCB…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AXC4T245 , SN74AXC1T45 , SN74AVC2T245 Hi,
For a new design using a Ultrascale FPGA from Xilinx and our automotive microcontroller I am about to use a voltage level shifter SN74AVC2T45 to convert…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AXC1T45 Hello,
The SN74AVC2T45 features Ioff partial power down isolation. Section 8.3.1 implies that either VCCA or VCCB can be a ground, which is typical of parts featuring Ioff.
Section…
Part Number: SN74AVC2T45 Hi ,
What is the state of I/O when there is no power to chip on both VCCA and VCCB pins?
When Input signal is available and when input signal is not available .
Regards
Dilip
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AVCH1T45 , SN74AXC1T45 , SN74AVC2T245 , , SN74AVCH2T45 , SN74AVC1T45 Dear support community,
We recently started a new project on a protocol which has to have a certain accuracy at high speed. …
Ok, thanks for your feedback.
In simulation, the OPA693 doesn't seem to adequately handle the required 200 MHz bandwidth. We have not yet tested the LMH6703.
Would a parallel level shifter setup like the SN74LXC8T245 or SN74AVC2T45 be suitable?
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AUC2G34 Hi Team,
Please advise us if SN74AVC2T45 could be used as a 1:2 clock buffer like below connection.
- No level translation. - Tie A1 and A2 together and connect 148MHz clock line.
Is…