Part Number: SN74AVC4T774-Q1 Other Parts Discussed in Thread: SN74AVC4T774 , SN74AXC4T774-Q1 , SN74AXC4T774 Tool/software: Hi,
I believe i may have found an error in the datasheet for SN74AVC4T774-Q1.
In this, in the sections highlighted, it specifies…
Part Number: SN74AVC4T774-Q1 Other Parts Discussed in Thread: SN74AXC4T774-Q1 Tool/software: Hi,
My customer is comparing SN74AVC4T774-Q1 to NEXPERIA 74AVC4T774-Q100. There are some differences in the electrical parameters and they have questions about…
Part Number: SN74AVC4T774-Q1 Other Parts Discussed in Thread: SN74AVC4T245 , SN74AVC4T245-Q1 Tool/software: We are using 74AVC4T774QPWRQ1(SN74AVC4T774-Q1 TSSOP Packeage) in our evaluation board.
There is no signal coming from the level shifter. I'd…
Part Number: SN74AVC4T774-Q1 Tool/software: I am having trouble with the evaluation board and would like to ask for your advice.
We designed and manufactured a PCB using SN74AVC4T774-Q1, and confirmed the VCCA→VCCB level shifter operation, but even…
Part Number: SN74AVC4T774-Q1 Tool/software: What is the delay when switching the direction pin from High to Low or Low to High?
I see OE to A/B delays, but nothing about delay when changing the direction pin.
Thanks. Mark
Part Number: SN74AVC4T774-Q1 Other Parts Discussed in Thread: SN74HCS151-Q1 , SN74AVC4T774 Tool/software: Hello,
I'm looking to use the SN74AVC4T774-Q1. Specifically orderable device 74AVC4T774QWBQBRQ1. This is the BQB (WQFN) package. The datasheet…
Hello Robert,
Unfortunately all of our 5V -EP level translators only have 1 DIR pin.
We only have a handful of devices that support individual bi-directional support, like the SN74AVC4T774-Q1 , but none support 5V inputs.
Regards,
Josh
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: TXV0106-Q1 , SN74AVC4T774-Q1 Tool/software: Though the datasheet claims speed of 310Mbps while converting 1.8V to 3.3 V signal, the measured data comes no where close to this. What could be…
Part Number: SN74AXC2T45-Q1 Other Parts Discussed in Thread: SN74AXC2T45 , SN74AVC4T774 Tool/software: Hi Expert,
Have a good day!
Do you have SN74AXC2T45(-Q1)’s 1.2V IBIS model?
Best Wishes,
Leo
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: LM63615-Q1 , ISO6520 Tool/software: Using the 74AVC4T774 with 3V on side A and 1.8V on side B. The side B 1.8V power is from a buck converter with 12V input.
This question is about the behavior…