Part Number: SN74AXC2T45-Q1 Other Parts Discussed in Thread: SN74AXC2T45 , SN74AVC4T774 Tool/software: Hi Expert,
Have a good day!
Do you have SN74AXC2T45(-Q1)’s 1.2V IBIS model?
Best Wishes,
Leo
Part Number: SN74AXC2T45 Tool/software: Hi team,
We are considering level conversion for the QSPI signal (1.2V → 1.8V). When SCK = 25MHz, can the SN74AXC2T45 be used for SCK level conversion?
Best regards,
Part Number: SN74AXC2T45 Other Parts Discussed in Thread: TXS0102 As titled, noticed DIR pin on the IC defines data direction from A to B or B to A.
Will it be suitable for I2C application?
And if not would you please advise if other devices could…
Part Number: SN74AXC2T45 Hi,
I would like to know the plating and underplating thicknesses for the SN74AXC2T45DCUR (VSSOP) version and for the SN74AXC2T45DTMR (2XSON) version. The composition is clear and the mass/ppm as well based on the documents…
Part Number: SN74AXC2T45 Hi Experts, May I ask for help? Our customer have a concern as shown belw: " I am looking into level shifter SN74AXC2T45 can't find hysteris spec on it" May we ask if you can provide this specification here for our customer? Thank…
Part Number: SN74AXC2T45 Other Parts Discussed in Thread: SN74AXC1T45 Hello experts,
I have two question about SN74AXCxT45.
1. Is it possible to apply same voltage for Vcca and Vccb?
In datasheet, there is description in below.
For example…
Part Number: SN74AXC2T45 Hello,
The customer wants to use SN74AXC2T45 1.2V to 1.8V level shifter. There is a description when 1.8V to 3.3V case as 380Mbps.
How fast can SN74AXC2T45 work when 1.2V to 1.8V case?
Best regards,
Toshihiro Watanabe
Part Number: LSF0204 Other Parts Discussed in Thread: LSF0108 , , TMUX1574 , TXB0304 , SN74AXC2T45 Tool/software: Hi team,
We are considering the LSF0108 and LSF0204 for level conversion with QSPI NOR FLASH. Are they usable under the following conditions…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AXC2T45 Tool/software: The device specification does not have a power supply tolerance specification. There is a table that suggests a tolerance "Pg 13" but it does not directly apply to a…