I found there are two different methods to calculate the maximum power dissipation for a device on E2E.
What is the different between these two methods?
Method 1:
Method 2:
Part Number: SN74AXC4T774-Q1 Hi team,
In the SN74AXC4T774QPWRQ1 data sheet, 6.13 states "Switching Characteristics, VCCA = 3.3 +/- 0.3V", in the table above, "tpd" when "B-Port Supply Voltage (VCCB)" is "1.2 +/-0.1V" is indicated as "min.0.5ns,…
Part Number: SN74AXC4T774-Q1 Hi,
In one of our projects, we used the level translator IC SN74AXC4T774QPWRQ1 as an replacement for SN74AVC4T774PWR in our production boards. We've observed failures with the level translator in our production boards after…
Part Number: SN74AXC4T774-Q1 I am using the LS1012A,
which is a 1.8V processor, and I want to connect the external interface to 3.3V.
So, I want to use SN74AXC4T774-Q1, but there is no GPIO in the application of TI homepage.
Can I use GPIO?
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: SN74AXC4T774 , TXU0304-Q1 Hi team,
I'd like to check with you that if we want to achieve SPI PCB inter-board communication and enhance SPI anti-interference ability, what is the cheapest…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: SN74LVC1G17-Q1 , TXS0108E-Q1 Hi Experts,
For below application, could you please recommend a cost-effective automotive voltage translator solution? I came up two ideas, which one is better…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: SN74LVC125A , SN74CBTLV3253 Hi team,
Do we have an IC similar to the SN74AXC4T774-Q1, except with four independent output enables (one per each of the four bits)? I was actually looking for…
Part Number: SN74AVC4T774-Q1 Other Parts Discussed in Thread: SN74AVC4T774 , SN74AXC4T774-Q1 , SN74AXC4T774 Tool/software: Hi,
I believe i may have found an error in the datasheet for SN74AVC4T774-Q1.
In this, in the sections highlighted, it specifies…
Tool/software:
I want to convert the level of an OD output signal through this level shifter, so I place a pull-up resistor at the input. However, this level shifter is a CMOS push-pull output.Does the output not require a pull-up resistor?