Part Number: SN74AXC8T245 Dear Team,
We are using SN74AXC8T245 in our design for 3.3V to 1.8V level shifting & We have below mentioned queries,
Could you please verify if the SN74AXC8T245 buffer is capable of supporting a 108 MHz clock signal? …
Part Number: SN74AXC8T245 Dear Texas Instruments Team,
I am planning to use SN74AXC8T245 in my design for voltage level translation.
My setup:
VCCA = 3.3 V (since OE and DIR Referenced to 3.3V)
VCCB = 1.2 V
I want to use it for SPI signals…
Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: SN74LXC8T245-Q1 , Hi Team,
I have a few questions regarding the SN74LXC8T245-Q1 and SN74AXC8T245-Q1 devices.
I am planning to use these devices for 3.3V-to-3.3V RGMII signals
For the…
Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: SN74AXC8T245 , Tool/software: Please tell me the values that are not listed in the datasheet for the device SN74AXC8T245 and SN74AXC8T245-Q1 .
I would like to know the maximum values …
Part Number: SN74AXC8T245 Tool/software: Dear product line application engineer,
my customer design in SN74AXC8T245 in his project. the VCCA power supply is 1.8V and the VCCB power supply is 1.2V. my customer has one question need consult: how much…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AXC2T245 , , TXV0108 , SN74AVC8T245 , TXV0106 Tool/software: Hi TI Team,
I am planning to use SN74AXC8T245 / SN74AXC2T245 to level shift from 1V2 to 1V8 for 1000Mbps GMII interface in my…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC541A Tool/software: Hi,
I want to use the SN74AXC8T245 as a buffer, here is the situation
1. the signals will first pass through an ISO67/ ISO77 digital isolator , 25MHz signals max…
Part Number: SN74AXC8T245 Was wondering if there is an analog IBIS model (non AMI) for the SN74AXC8T245 or any similiar CMOS 245? Will be using to sim a 245 to 245 on a long parrallel multi drop bus and want to look at settling times. Thanks Tom
Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: TXV0108 I need to level translate from 1V8 to 3V3. SN74AXC8T245PWR supports upto 360Mbps. I need IC with better bandwidth, maybe more than 400Mbps. Do you have anything similar with dir control…