Part Number: SN74AXCH1T45 Hello,
Our customer has a question about product differences between SN74AXCH1T45DRYR and SN74AXCH1T45DRY2.
Could you let us know the differences between two devices.
Best regards,
Part Number: SN74AXCH1T45 Other Parts Discussed in Thread: SN74AUC1G125 , CDCBT1001 I'm posting on behalf of my customer: Do you recommend SN74AXCH1T45 for 25Mhz output, rise/fall time <=1ns application? Also, we assume that this IC can supply 12mA output…
Part Number: SN74AXCH1T45 Tool/software: Hello
Voltage translator from 3.3V to 1.8V
Direction is from A to B
1.8V 10Kohm PU resistor
Input is Hi-Z (without PU)
Why output is 0V after power up ?
Attached schematic drawing
Thanks !
Part Number: SN74AXCH1T45 Hi, i saw your discussion about the missing SN74AXCH1T45DRYR package dimension. You mean we have already update the datasheet. But i still can find the information in new download datasheet(still 2020) beta. Would you please…
Part Number: SN74AXCH1T45 Hi,
We are using SN74AXCH1T45DCKR in our design to convert 50MHZ and 100MHz clock signals from 3.3V to 0.75V level.
We we tested this section on the board, we see that the signal towards 0.75V side is around 200mV level and…
Part Number: SN74AXCH1T45 Hi Experts,
Good day.
We would like to ask if this 1-bit translator device SN74AXCH1T45DRY can efficiently translate 2.5V to 1.2V signal at 12.5Mhz?
Are there any better solution for this rate of conversion?
Its datasheet…
Part Number: SN74AXCH1T45 Hi Team,
I cannot find the DRY dimension information in datasheet. Could you please help to provide it? Thanks.
Best regards,
Hardy
Part Number: SN74AXCH1T45 Other Parts Discussed in Thread: SN74AXC1T45 , SN74AUC1G74 , 74AVC1T45 , SN74AVC1T45 , SN74AUC1G125 What is the maximum speed at which SN74AXCH1T45 or SN74AXC1T45 can toggle at when supply is 0.65V?
That is what is the rise…
Part Number: SN74AXCH1T45 Hi Team,
We cannot found the respond time with differential VCCA/VCCB in the datasheet. Look like closest information is Table 6-1 -Table 6-8 but the title of column is not shown.
Could you please provide completed table…
Part Number: SN74AXCH1T45 Other Parts Discussed in Thread: TUSB2E22 Hi Experts,
Good day. Is this device also supports 1.2V to 3.3V level translator up to 500Mbps? Info sheet only shows 1.8 to 3.3V.
Please confirm.
Thank you for your guidance. …