Part Number: SN74LV32A The datasheet has the following regulations as electrical characteristics. ・ ∆t / ∆v Input transition rise or fall rate : -VCC = 3 V to 3.6 V: 100ns / V (MAX) When the above time was measured (*) with the product mounted on our board…
Part Number: SN74LV32A
I would like to make sure below 2 devices TjMax. = 150 ?
SN74LVC1G125DCK
SN74LV32APW
Thank you for your kind help
Best regard
Yuki
There is no such automotive-qualified device. You have to combine multiple OR gates; 3× 3 inputs (SN74HCS4075-Q1), or 4× 2 inputs (SN74LVC32A-Q1, SN74HCS32-Q1, SN74AHC32Q-Q1, SN74LV32A-Q1).
Hi Mayank,
Is the purple signal at the output of the SN74LV32A? (looks like it would be TP26 in your design)
If that signal is from the SN74LV32A, I would suspect that the low-state driver at the output is damaged and you need to swap out that device…