Reposting the list of devices with GPNs as the answers wont change between package types or quantity
SN74AC74 SN74AHC1G32 SN74AUP1G99 SN74LVC04ASN74LVC04APWTE4
SN74LVC125A
SN74LVC126A
SN74LVC1G07
SN74LVC1G08
SN74LVC1G14
SN74LVC1G97
SN74LVC1G99…
sn74lvc04a.pdf Hi Wade,
Can i load 64mA on each output(in the low state) so that the total current into the ground pin will be 256mA? Is there any limitation on the ground pin current(not given in data sheet)?
For example , if we take sn74lvc04a …
Hello,
Short answer: You need a logic inverter such as SN74LVC04A -- assuming your signal is 0V for a low and 3.3 or 5V for a high.
Long answer: I will need your help in getting some info for the signal you want to invert to be certain of what you…
No. The board default setup uses the SMA for the input clock. If you plan on using pin 39 you must make the following changes to the board.
install R34
remove T2
remove R12
install C55
You can send the 1.8V source to both J12 and J14.
You…
Hello,
A couple comments:
Is there a short on the output?
Is the output pulling a lot of current?
Is the input fully down to 0V at the device?
These are a few things that could be messing up the operation of the device.
If there really is no…
Hi Tommy,
The TRM describes the voltage differences between both SD/MMC interfaces. You can use as reference AM/DM 37xx Hardware user guide:
The EVM supports two SD/MMC interfaces • SD/MMC1 with 1.8V/3.0 V support • SD/MMC2 with 1.8V support only…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage Translation FAQs - All-Time
How does a slow or floating input affect…