Part Number: SN74LVC07A-Q1 Hi Team,
My Customer is looking for the Slew rate of SN74LVC07A-Q1. This is not indicated in the datasheet and I can't find that information either. Can you share information about this?
Regards, Renan
Part Number: SN74LVC07A Hello,
Since we found the failure on the SN74LVC07A on UPS application,
Could you kindly help to comment!
1. Please help to check if the schematic is ok or not as enclosure?
2. The input signal of the buffer is from DSP GPIO 3…
Part Number: SN74LVC07A Hi,
Just wondering if SN74LVC07ARGY (QFN) thermal pad is internally connected to GND and can increase max total GND current?
Thanks.
Part Number: SN74LVC07A Hi
We are using SN74LVC07A in many of our applications as buffers as well as voltage shifter from 3.3 to 5V. However we are facing a lot of failures in these ICs and as such are not able to understand the reasons. For e.g. we are…
Part Number: SN74LVC07A Other Parts Discussed in Thread: TPL7407LA
I'm using the SN74LVC07APWRG4 parts.
They are powered with 3.3V. The open drain is needed. But I noticed in the datasheet it says that the "Recommended Output Voltage" is 5.5V max.…
Part Number: SN74LVC07A-Q1 Other Parts Discussed in Thread: SN74LVC07A , Hi, Team:
What's SN74LVC07A supported maximum frequency?
The background is we DIN SN74LVC07A-Q1 in Visteon project as IIS level shift from 1.8V to 3.3V which using12.288MHz MCLK…
Part Number: SN74LVC07A Hi Team,
My customer is asking the input impedance of SN74LVC07A, it is not listed in datasheet may I have this information?
Thanks a lot.
Vincent Chen