Part Number: SN74LVC1G125-EP Other Parts Discussed in Thread: SN74LVC541A-EP , SN74ACT244-EP , SN74LVC541A
HI,
I need to understand HBM ESD rating for the following three devices:
SN74LVC1G125-EP (orderable: CLVC1G125IDCKREP)
SN74LVC541A-EP (orderable…
Part Number: SN65HVD1050-EP Other Parts Discussed in Thread: SN74LVC1G125 Hi
I like to use the CAN transceiver, SN65HVD1050-EP.
The datasheet shows "Reference output voltage is 0.4Vcc~0.6Vcc".
Does it mean that this VREF is an output pin?
If…
Other Parts Discussed in Thread: SN74LVC1G125-EP Dear all,
I would like to know what would happen if, under a failure condition, the input for SN74LVC1G125-EP goes up to 28V while keeping the the supply regulated to 3.3V.
I assume the device will break…
Part Number: SN74LVC374A-Q1 Other Parts Discussed in Thread: SN74LVC1G125-EP Hi E2E,
Good day!
A customer of mine is asking if SN74LVC374AQPWERP and SN74LVC1G125-EP can tolerate 11 volts for maximum 120 us at the output pin while the output(s) are tri-stated…
Other Parts Discussed in Thread: LSF0108 , SN74LVC1G125 , SN74AVC16T245 , SN74LVC2G125 , SN74LVCH16T245-EP , SN74HCT244 Hello,
My application calls for a Bi-Directional voltage translator Buffer with the following parameters. On the low voltage side +3.3V the…