Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: SN74LVC2G17
Hi
Our customer are considering to use this device for cable driver which is coaxial cable.
And the input signal is a SIN wave (condition: Fin=100MHz, Vin_pp=3Vpp, Vcm=…
Part Number: TCAN3414 Other Parts Discussed in Thread: SN74LVC1G125-Q1 We are looking for a CAN transceiver (3.3V) that has a low power enable but also tristates the receiver output. The TCAN3414 or SN65HVD234DR both have low power disables but the receiver…
Other Parts Discussed in Thread: SN74LVC1G125-Q1 Hi Team,
Please review the SCH as attached.
I have one question.
The Vcc =5V, SET is 0V / 5V. A = 5V to 5.3V
SET=0V, B0 is turn-on at A=5V
SET=5V B1 is turon-on at A=5V. but A is changed to 5…
Other Parts Discussed in Thread: SN74LVC1G125-Q1 Please tell me SN74LVC1G125-Q1 out of "Y terminal".
is "Y terminal" a high impedance at the time of Vcc=0V, OE=GND, and A terminal = Low?
Part Number: SN74LVC1G07-Q1 Other Parts Discussed in Thread: SN74LVC1G17-Q1 , SN74LVC1G125-Q1 Tool/software: Hi Team,
I had tested the non inverting open drain buffer SN74LVC1G07QDBVRQ1 with 10K pull up resistor connected to 3.3V and 3.3V supply given…
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: TPS6594-Q1 , SN74LVC1G125-Q1 Tool/software: Hi,
Project Name : RN PCU
Buffer/lever shifter : CAXC4T774QRSVRQ1
schematics implemented as below
buffer supplied with the 3.3V and…
Hi Amit,
You are asking for a functional safety document for a non-automotive device.
I can create it for the Q1 version of this device (SN74LVC1G125-Q1).
Generally, commerical devices are not functional safety rated.
Below the minimum recommended supply voltage of 1.65 V, correct operation is not guaranteed. In particular, the output will not be able to drive low as long as the gate threshold voltage of the internal MOSFETs has not yet been reached.
Devices with…
Part Number: SN74HCS21-Q1 Other Parts Discussed in Thread: SN74LVC1G125-Q1 , SN74LVC1G126-Q1 , SN74LVC1G99-Q1 , SN74HCS21 Hi Expert,
I'm verifying the "AND" logic IC SN74HCS21-Q1 for our project. I found an abnormal phenomenon from this chipset. Showing…
You do not need level translators to prevent leakage. It is enough to use a plain buffer with overvoltage-tolerant inputs and/or I off , e.g., SN74LVC1G125-Q1.