Part Number: SN74AUC2G04 Other Parts Discussed in Thread: SN74AUP2G17 , SN74LVC2G34 , SN74LVC2G04 Hi,
I am using 2 Pin Bicolor LED where reversing polarity change its color.
Supply Voltage :3.3V
LED Specifications are
Forward Voltage: 2V
Max Current: 2…
Part Number: SN74AUC2G04 Other Parts Discussed in Thread: SN74AUP2G04 , SN74LVC2G04 Hi,
I have two questions:
1) For SN74AUC2G04YZPR inverter, what should be the approximate Vin_l at 3.3V VCC. What should be its approximate Vin_l value at 2.7V VCC.
2)What…
Good morning,
Thanks a lot again for all information. Let me summarize my application again.
FPGA ---3V3 signal--> LVDS Driver(sn65lvds31) ---LVDS--> LVDS Receiver(sn65lvds33) ---3V0 signal--> Level shifter(sn74lvc2t45)--5V signal--> Inverter(SN74LVC2G04…
Part Number: MAX232 Other Parts Discussed in Thread: SN74LVC2G04 Hi team,
My customer is going to connect T1OUT to T2IN and R1OUT to R2IN to invert the signal.
Could you check it will not cause the damage of device?
Regards,
Saito
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74LVC2G04 , SN74LVC1G06 Hello Guys,
Good day.
Our customer is looking for the IBIS model for SN74LVC2G06. However this is not available. Can he use the IBIS model from SN74LVC2G04 ?
Is there any…
CDxxx devices were acquired from Harris Semiconductor; I doubt that TI would have more information than what is already published.
For all TI logic devices, channel-to-channel skew is less than 1 ns. As far as I know, device-to-device skew data is usually…
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: SN74LVC2G04 , SN74AHCT1G04 , LSF0102 I am looking for a component to replace the functionality of these two components, level shifter sn74lvc2t45 and inverter sn74lvc2g04. Data sheets are attached…
Hi Jerry,
The customer service system and the E2E (Engineer to Engineer support forums) are not connected.
I see that you want to get thermal metrics for 5 devices from my group (standard logic):
SN74LVC1G125 - DSF
SN74LVC1G74 - DQE
SN74LVC1G126 - D…
There's isn't an application report, however it seems like a very simple solution. This is how I would do it:
Something like an SN74LVC2G04 should do the trick. In this case, one of the LEDs will always be on.