Part Number: SN74LVC2G08-Q1 Hi ,
I am using SN74LVC2G08-Q1 in my project application and I while validation I find some discrepancy in the output waveform. I have provided IN1 = 3.3V and have provided a triangular waveform with 10kHz at IN2. We can…
Part Number: SN74LVC2G08-EP Hi team, I'd like to know about the difference between SN74LVC2G08MDCUREP and SN74LVC2G08DCUR. According to the datasheet, ”t PD" seems to be different. Sincerely. Kengo.
Part Number: SN74LVC2G08 Hi TI team, as per page 5 in datasheet of SN74LVC2G08 it is said the input transition rise or fall rate is 10ns/V maximum. May I know why the AND gate has this limitation? Does it mean the slower transition rate has any bad effect…
Part Number: SN74LVC2G08 Dear Sir/Madam,
According to the SN74LVC2G08DCUR datasheet, can i say the tolerance for the DCU VSSOP package should be in between 3.00 to 3.2 mm.
One of my customer is having this 2 body marking but the observed length…
Part Number: SN74LVC2G08-Q1 Hi ,
We are using SN74LVC2G08QDCURQ1 in our project application.
I tried measuring input leakage current of the device at 25 deg and it was around 8.6 uA, while at -40 deg it is 300uA.
Is there any relation between input…
Part Number: SN74LVC2G08-Q1 Other Parts Discussed in Thread: TLV9032-Q1 I am looking for pin drop replacement for my existing part 74HC2G08DC-Q100 (NEXPERIA) in one of my design. At present i am using it for just driving transistor base with 100k and…
Part Number: SN74LVC2G08-Q1 Hello
According to the following information , the SN74VCG08QCURQ1 is preview ,and is the PCLV2G08QDCURQ1 as same as SN74VCG08QCURQ1? I need a Dual 2-Input Positive-AND Gate used in the automotive industry, temperation range…
Part Number: SN74LVC2G08 Hi team,
For the DCT package, I'd like to varify why catalog part temp range is -40 to 125, and automotive part temp range is only -40 to 85? Is there anything wrong?
Thanks.
Part Number: UCC21520 Other Parts Discussed in Thread: SN74LVC2G08 , Hello!
I am using the UCC2150 to manage a H-BRIDGE connected to a brushless motor (Power side).
To attack H(INA) and L(INB) inputs (isolated signal side) i am using a logic to decode…