Other Parts Discussed in Thread: SN74LVC2GU04 Hi,
I'm working on a design that involves a PWM signal with a carrier frequency of ~1-3MHz 0 and 5V and I've been trying to use the SN74LVC2GU04 to invert the signal. I've scoped the input to the…
All modern logic devices have input buffers with a small amount of hysteresis, which makes it hard to use them as linear amplifiers.
To allow feedback, you need to use unbuffered inverters (SN74LVC2GU04 or SN74AUC2GU04).
However, to buffer the output…
Hi Anjali,
There are no parts in our logic portfolio that are going support 24V. I would suggest using a Step-down(buck) converter to connect to the inputs of one of our inverters
Ex: SN74LVC2GU04 or SN74LVC2G14.
Regards,
Sebastian
Part Number: CC2652R Other Parts Discussed in Thread: SN74LVC2GU04 , Tool/software: WEBENCH® Design Tools I have a question for AOA reference circuit of BOOSTXL-AOA Evaluation board. there are six antennas and TI logic Ic (SNSN74LVC2GU04 or SN74LVC1G08DCK…
Part Number: TPS75003 Other Parts Discussed in Thread: SN74LVC2GU04 , TPS3803 , Hello,
Are you able to tell me if the following part numbers: TPS75003; TPS3803-01DCKR; SN74LVC2GU04DCK have any FCC markings?
Thank you!
This is very useful information, thanks.
Would you than recommend using SN74LVC2GU04 for this application ?
I could also use SN74LVC1GX04, but the package is too big for our actual design.
Thanks
Yan
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…