This is no problem if V CCP = 5 V. (The pull-up voltage must never be above V CCP .)
The pull-up resistors have an effect only shortly after power up when the I/Os have not yet been configured as outputs. The value of the pull-up resistors does not really…
Hi Tosi,
You can place sn74lvc3g14 from the part search:
For SDM03U40, please follow this video:
PSpice for TI: 3rd Party Model Import | TI.com Video
J5 looks like a connector, I don't think you need to simulate it.
Thanks, JC
Fairchild's VHC and TI's AHC are pretty much equivalent, and support 70 MHz at 3.3 V.
There is no faster drop-in replacement. For different packages, look into the LVC family (e.g., 2× SN74LVC3G14).
What is the problem with the 74VHC14MX…
Hi Jeril,
I understand the urgency. I want to assure you we're working on your issue with priority. I want to ask about the inverters you're using (SN74LVC3G14) on your RESET, WDO, and PFO lines. My question is, why are you using these? Are you trying…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: LMH6881 , , SN74LVC1G14 , SN74LVC2G14 , SN74LVC3G14
Hi team,
Need to level shift a 0V logic 0 reference to -1.25V logic 0 reference for the LMH6881 device SPI working with max 50MHz SCLK frequency…
Part Number: SN74LVC3G04 Other Parts Discussed in Thread: SN74LVC3G14 , Hello,
I want use SN74LVC3G14 as a Level shifter. (Vcc=5V)
- When I stet the Input to a 5V Level everything is Ok (Icc = 55uA)
- But when I set the Inputs to 3,3V-Level the IC needs…
Part Number: SN74AHCT14 Other Parts Discussed in Thread: SN74AUC14 , SN74LS14 , SN74LVC14A , SN74LVC3G14 Hello,
I'm considering replacing Toshiba Logic TC74VHCT14AF (SOP package). SN74AHCT14 (NS package) is hit in TI cross reference. I'd like the 5 V (input…
We do not have any models for this part and dont have the data to create one since they are so old.
Here are some other options. SN74HC14 still no models
SN74LVC14 Has IBIS model and can create HSPICE if needed . I will need name, company info, and…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…