Part Number: SN74LVC8T245-Q1 Dear TI,
We are using in one of our products the following component: www.ti.com/.../SN74LVC8T245-Q1 When opening the product's datasheet mentioned on above webpage we get this orderable part number: SN74LVC8T245QPWRQ1,…
Part Number: SN74LVC8T245-Q1 Hello.
I would like to inquire about the marking information for the this part number.
SN74LVC8T245QPWRQ1
The product marking consists of 4 lines.
--marking--
NH24Q
TI 62K
A TL C
5m
----------
The last…
Part Number: SN74LVC8T245-Q1 Dear team,
i require SN74LVC8T245-Q1 PSpice model to simulate in LTSPICE XVII,Please share the model file asap.
Best regards,
Navya.d
Part Number: SN74LVC8T245-Q1 Dear TI experts,
Can I get Functional safety report of SN74LVC8T245QPWRQ1?
(Including Failure Mode and Failure Distribution Rate)
I cannot find it on product page.
If you do not have the document, please just check…
Part Number: SN74LVC8T245-Q1 Other Parts Discussed in Thread: SN74LVC125A Tool/software: Hi team,
Can you please check if there is buffer in SN74LVC8T245QPWRQ1? We see it in SN74LVC125A.
Part Number: SN74LVC8T245-Q1 Tool/software: Hi,
According to the datasheet of SN74LVC8T245-Q1, not mention it pass AEC-Q100 qualification, also for target EE, not mention automotive. my customer want to know if this one has passed automotive related…
Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: SN74LVC8T245-Q1 Hello,
Could you help check and advise the difference between SN74LVC8T245-EP and SN74LVC8T245-Q1?
Except the operating temperature range, is there any other difference…
Part Number: SN74LVC8T245-Q1 Tool/software: Hi experts,
As a LVC logic, I noted this part input is 5V tolerant (absolute maximum input is -0.5V to 6.5V, no related to VCC voltage). So if this means I can use it implementing 5V logic to 3.3V logic translation…
Part Number: SN74LVC8T245-Q1 Hello, Are you aware of any conditions such as supply noise or brownout condition that would cause the direction to swap from B->A to A->B erroneously given below schem? Decaps are of course, placed close to device and solid…