Part Number: SN74LVT8996 I have 6 of the devices on a backplane and would like to fine a way to test all the connections and addressing.
Presently I do a bit bang to from a vector test with LabView and one of there 96 I/O cards, but it is hard to use…
Part Number: SN74LVT8996 What about the max operating junction temperature?
Noted that 150degC is the absolute maximum but it could most likely be storage ?
Part Number: SN74LVT8996 Other Parts Discussed in Thread: UCD9090-Q1 , UCD9090 , , Hello,
My customer is using SN74LVT8996-EP in a design with the UCD9090-Q1 as the JTAG device. The UCD9090 calls for a 10kOhm external pull down on the /TRST line, but the…
Part Number: SN74LVT8996 When I scan all the TAPs on my JTAG Bus, one of them answeres with " I-S-10xZERO-S-I "
So far I know, this is the code for a Reset of the device. What can be the reason to induce the SN74LVT8996 to answer with this code…
There are several options available to you.
You can use a LASP, or a multidrop addressable.
Please see below for jtag products.
http://www.ti.com/lsds/ti/logic/boundary-scan-jtag-logic-products.page
The SN74LVT8996 or one of the multidrop devices.
Regards…