Part Number: SN74LXC2T45SN74LXC2T45DCUR
The part has a top marking of 2LDT
However, the datasheet does not have any details for this part, so we cannot confirm if this is correct or not.
Can you please confirm the top marking is correct.
Many…
Part Number: SN74LXC2T45 Tool/software: Hi
We are looking the part SN74LXC2T45 for signal level translation. Propagation delay is our key parameter for design.
There is given Minimum propagation delay (with VCCA= 3.3 ± 0.3 V) as 1ns and Max propagation…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: SN74LVC2T45 Tool/software: Hi Josh
Thanks for update..
What are the conditions to get propagation delay as minimum 1ns as mentioned in datasheet of this part (SN74LXC2T45).
The propagation…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: LSF0101 Tool/software: We are currently working with the SN74LXC2T45 dual-bit level shifter in our design and needed to simulate its behavior. Since an official SPICE model does not appear to be…
Part Number: SN74LXC2T45 I am using the level shifter SN74LXC2T45 with two 3.3V power supplies. However, the input signals to the level shifter are 5V. Is there a risk of damaging the component?
Part Number: SN74LXC2T45-Q1 Tool/software: When the SN74LXC2T45-Q1 chip is in use, if the input pins are left floating, what kind of impacts might this bring about?
Part Number: SN74LXC2T45 Tool/software: Hello,
I have a customer whom ordered P/N: SN74LXC2T45QDTTRQ1
qty. 50
The customer's main inquiry regarding the part they received was that the markings they got had part marking : 1LN instead of ILL which…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: SN74LXC1T45 Good morning
Can you kindly suggest the Level shifter for the below mentioned Requirements
Output current – 32mA max
Non-isolation
Communication Procedure - Start-stop synchronous…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: TXU0202 , Hello ,Good Morning
Can you kindly suggest the Level shifter for the below mentioned Requirements
Non-isolation
Communication Procedure - Start-stop synchronous (Asynchronous…
Part Number: SN74LXC2T45 Other Parts Discussed in Thread: SN65EPT21 Tool/software: Hi team ,
I hope you're doing well.
We have confirmed the use of the SN65EPT21 device in our design and are currently preparing for simulation. To proceed, we would…