Part Number: SN74V263
Tool/software:
Hi,
I'm working on a project using the SN74V263 FIFO in standard mode with a 9-bit input and output bus width. I'm facing an issue with my write and read operation and the status flags.
My system uses an external…
Part Number: SN74V263-EP Tool/software: Hi, Is the read clock buffered internally in the device? Could I run the clock using a sine wave an trust that an internal schmitt trigger would square the clock?
Part Number: SN74V263 Hello,
We need to switch to the SN74V263-6PZA from the SN74V263PZAEP. Can the SN74V263-6PZA operate at 133MHz as well?
The datasheet only mentions a max clock frequency of 166 Mhz.
Thank you and best regards,
Ambroise
Part Number: SN74V263 We are looking to replace the CY7C4255V-10ASC which is now obsolete with the TI SN74V263 but need to know how long this part will be available.
Thanks,
Tom
Part Number: SN74V263 We are looking to replace the Cypress CY7C4255V with the SN74V263. One issue that has come up is the retransmit pulse in standard mode. Fig 11 of data sheet shows that you need to wait until EF goes high before bringing REN low.…
The application intends to make use of SN&$V263 FIFO, where 9 bits wide input and output buses are used. And the "writes' after which the FIFO will assert the Full Flag is 16384. The "half full" flag will be asserted at 8193rd write.
At the time when…
Vasudevan,
Unfortunately, we did not create or publish IBIS models for this device.
However, the SN74V263 series of fifo uses the same output buffers and can be used in place of the SN74V3680
This model can be found here: www.ti.com/.../toolssoftware…
Part Number: SN74V273-EP Hello,
I am a Computer Engineering Junior and am currently working on a design team working to build a cubesat that is set to launch in 2019. We are currently working to make two SN74V273-EP memory chips working on a board we…
Other Parts Discussed in Thread: SN74V263-EP Dear TI-Team,
for our application we need to connect a 16Bit parallel camera to the 8Bit DM37x camera interface.
We found a solution and I need confirmation regarding its practicability.
The idea is…