Part Number: SN74V293 This is a follow-up to issues that were posted a few months ago regarding a mismatch between data written to the SN74V293 and data read out from it.
Hopefully the link here will properly redirect to it.
In this application, some…
Part Number: SN74V293 Hello TI Community,
After looking through the SN74V293-X datasheet, I don't see any reason that I can't drop the variants allowing for a higher maximum clock in place of those allowing for a lower maximum frequency clock.
Is…
Part Number: SN74V293 I have an application where a 74V293 is connected between a microcontroller and a parallel DAC to provide an "elastic" buffer between the two, and to enable the data to the DAC to be transferred at a well-controlled rate.
I've…
Part Number: SN74V293 Hello,
I have a problem with my SN74V293 FIFO. I'm not able to readout the memory although I use the timing information for the clock and signals from the data sheet. The inputs of the FIFO are connected to the outputs of a 12…
Part Number: SN74V293 I have a number of prototype boards that incorporate 'V293 FIFOs. During configuration, firmware verifies the operation of components on the assembly, including the FIFOs.
The previous version of the prototype (using 'V293s with…
Other Parts Discussed in Thread: SN74V293 , MSP430FG4618 Hi,
Anyone have a C code to test the operation of the FIFO (SN74V293) on a microcontroller MSP430FG4618? My project is to receive a signal transducer 500KHz, transform the analog signal to digital…
On page 16 of the SN74V293 datasheet notice that there is no minimum frequency, nor any maximum high or low time for the clocks. Would you like me to transfer this thread to the logic forum where they can give you more information about the SN74V293?…
Part Number: SN74V273-EP Hello,
I am a Computer Engineering Junior and am currently working on a design team working to build a cubesat that is set to launch in 2019. We are currently working to make two SN74V273-EP memory chips working on a board we…
Other Parts Discussed in Thread: TUSB3410 , MSP430FG4618 , SN74V293 Hi,
I have on my board IC's
MSP430FG4618, TUSB3410, TPS79501 (regulator) and 24LC128 (EEPROM). I wonder if the card to
connect to the computer via the USB cable the computer will…
Other Parts Discussed in Thread: ADS5562 , SN74V293-EP , THS4151 , ADS5560 Hi!
We are using 6 ADS5562 on one PCB with the following configuration:
Normal
0
21
false
false
false
DE-AT
X-NONE
X-NONE
…