Part Number: SN75175 Hello guys,
One of my customer uses SN75175 for their current products.
Recently, they knew SN75175 datasheet was updated from version SLLS145C to SLLS145D. At this moment, they have the following questions. Could you please give…
Part Number: SN75175 Other Parts Discussed in Thread: AM26C32 , AM26LV32 Hi,
We are looking at the SN75175 for a product that will receive either or a RS422 or single ended TTL (5V.) We will need to handle either option on the same input port/pins.…
Part Number: SN75174 Other Parts Discussed in Thread: SN75175 Hi Team,
I have some unused channels for the SN75174 Line Driver and SN75175 Line Receiver, and I wanted to confirm how to connect the pins of these unused channels.
The datasheet didn…
Part Number: SN75175N
The MSL rating for SN75175N is listed as Level-NC-NC-NC. In a similar forum, I found that this means there is no moisture rating as moisture cannot ingress into the package. Would it be fair to say in other words that the relative…
Other Parts Discussed in Thread: SN75175 , SN74LS240 Hello,
Our customer uses the SN75175.
The customer wants to know the absolute maximum ratings about output terminal.
It is mentioned the Low-level output current on the datasheet. But there is…
Other Parts Discussed in Thread: SN75175 , AM26C32 , AM26LV32E Hi,
I am working on SN75175. I didn't connect the inputs and outputs, just VCC, GND and EN pins are connected.
In this case supply current is about 50 mA.
Then I connect inputs VCC and…
Part Number: SN75173 Other Parts Discussed in Thread: SN75175 Tool/software: Looking for a IBIS model of SN75173D, or an suggest an equivalent alternate IBIS model part for the same.
Part Number: MC3486 Other Parts Discussed in Thread: DS34LV86T , SN65LBC175 , DS34C86T , AM26C32 , AM26LV32 , SN75175 Tool/software: I am looking for an alternative for the MC3486, that has a lower power consumption and is P2P, if possible.
Part Number: SN7400 Other Parts Discussed in Thread: SN75159 , SN75175 , SN65LBC175 , MC3486 Tool/software: Hello there,
The following TI components have gone obsolete. Can you please suggest the replacements for the same.
1) LH0070-2H
Description…
Hello, I think my problem is (partially) solved. Using quadruple differential line receiver SN75175 and following circuit c) Isolated Power Supply / SN75175 Vin = Vcc_PowerSupplyOut = 5V / 7V / 9V /12V Vcc = Vcc_SN75175 = 0V or 5V Receiver Enable = high…