Part Number: SN75374 Hi exparts,
According to the datasheet, the recommended operating conditions are IOL=40mA (low-level). Is it unusable if it exceeds the recommended use conditions (for example, 125mA)? The peak output current (II) is 500mA (TW …
Part Number: SN75374
Hi exparts,
Could you tell me a driver which has higher sink current(>60mA) than SN75374 but same function. I prefer p2p with SN75374. If there is no p2p device, please let me know some devices with smaller PCBA.
Regards, H…
Part Number: SN75374 Other Parts Discussed in Thread: UCC27444 Tool/software: I'm looking for the similar function with MIC4468 for the 5V to 12V with individual disable function. Could you help to check if any similar one or not?
Regards
Brian
Part Number: SN75374 Hi team,
There are 4 questions related to power supplies as the attached.
SN75374.pptx
Could you support this?
Regards,
Noriyuki Takahashi
Part Number: SN75374 Hi TI.
I am currently evaluating the circuit using the SN75374, but I would like to know about the internal circuit of this IC.
(1) When wiring is performed as shown in the attached circuit diagram SCH1 and the 5V power supply…
Part Number: SN75374 Hi Ti.
What's diffrence betwee SN75374D and SN75374DE ?
Additionaly, what's diffrence betwee SN75374DR and SN75374DRE and SN75374DRG ?
Sincerly.
Yuzuru.
Part Number: SN75374 We are using SN75374 for our fan control circuitry. The connections and schematic is shown in attached file (Image-1). The output of SN75734 which is labelled as Fan_pwr_con-1-OUT etc is used in another IC named FDC3601N (Image-2…
Other Parts Discussed in Thread: SN75374 Please let me know about three point below of SN75374.
---------------------------------
①When Input, Enable, and Vcc1~Vcc3 are supply below voltage,
I think that current path are below red line, is it correct…
Hi Kent ,
do you think TPL7407 would work in your application ? I used the below compare tool for selecting this .
sn75374 also is an option which has enable pins to control output state.