Hi all,
This chip is connected to a xilinx FPGA which I am going to implement my IP core. My problems are,
1. To use the HDMI output do we have to input TMDS signals to the chip?
2. Does this IC have internal DP-to-TMDS converter ?
Thank you
Other Parts Discussed in Thread: SN75DP126 , SN75DP130 Hello,
I have a question, I have been searching for the right product the last few days and not sure if the above are the right ones.
I want to use a Displayport connector and connect this one to one…
Other Parts Discussed in Thread: SN75DP126 , SN75DP139 , TMDS261B , HD3SS215 Hello,
SN75DP126 chip have two outpus TMDS Output1 & DP Output2.
Instead of using the DP output channel can I use it as TMDS output? so the chip will support two TMDS…
Part Number: SN65DP159 Other Parts Discussed in Thread: SN75DP126 ,
Hi,
Am planning to use SN75DP126 chip of DP++ (DDI) input and DP1.2 HDMI1.4b output.
As per SN75DP126 chip spec, SN75DP126 have in built-in level translator for HDMI 1.4b.
My question…
Other Parts Discussed in Thread: SN75DP129 , SN75DP122A , SN75DP139 , SN75DP126 , DM3730 TI is having any processor which can convert Displayport 1.2 input to DVI output
Other Parts Discussed in Thread: SN75DP126 Hi,
Is there an IBIS model available for SN75DP126 ? This is for a simulation in Hyperlynx 9.2. If not can you please provide me a IBIS with similar properties?
Thank you