Part Number: SRC4184 with 25 MHZ RCK reference clock, LRCK input at 48K, LRCK output at 44K and getting garbage data for converted output. Slave Mode, all config pins grounded.
Hardware mode. Shouldn't READY output go low once input/output clocks are…
Other Parts Discussed in Thread: SRC4184 , SRC4192 Hi,
Our system requires interfacing Bluetooth module audio to and audio mixer using I2S interface. The Bluetooth module support only 8KHz sampling rate with 16-bit data width over a 24/32-bit frame (I2S…
Other Parts Discussed in Thread: SRC4184 Hi One of our application using SRC4184 & it is using software control mode. Can i leave open all configuration pin (LGRPA, LGRPB, OFMTA, OFMTB) or should i need to connect it vcc or ground.SRC
Hi,
If they do not need ADC/DAC and just looking for interface devices then possible option:
2 pieces of SRC4382 or SRC4392: These devices integrate only 2 Channel SRC’s and S/PDIF so we will need two of them.
SRC4184/SRC4194 + DIX9211/DIX4192 …
A customer asks:
On the SRC4184 , do I need to force the MUTEA and MUTEB input pins low or is there a sufficient internal pulldown that would allow me to leave these floating?
Other Parts Discussed in Thread: SRC4184 Dears
Could you please help to provide SRC4184 IBIS Model to me, one of my key customer need it for simulation.
Thank you very much!
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4184 , , SRC4194 Hi, Team,
My customer is looking for SRC which can convert 48khz from 32kHz, 44.1 kHz or 48kHz. Theare are 2 I2S data line. I means the customer would like to drive 4 speakers.
Could…
Dirk,
Unfortunately I don't know of any readily available ASRC libraries from TI. I believe you would either need a separate IC such as the SRC4184 or would need to license an algorithm from a 3rd party.
Can you supply some more info about the signals…