Part Number: DS560DF410 Tool/software: Hi team, Please help to recommend suitable devices (P2P would be better) to replace DS560DF410. The datasheet of competitor as below. Thanks. DAVICOM-DM9162.pdf
Best Regards, Ryker
thank you for your answer, i followed this guide, after installing Graphics SDK to my file system. I run /etc/init.d/335x-demo after bootup, here is the script
0x10205 release8.x installing 8.x SGX release user libraries Installing PowerVR Consumer…
The latest version (on line @ ti.com) of the DP83822 datasheet seems to have the missing dimension issue as well. I've attached an older version datasheet from 2019 that has the mechanical details of the package. From page 112 of SNLS505E, please compare…
I'm a complete newbie to CCS and the 6713DSK (This is the board I am using http://c6000.spectrumdigital.com/dsk6713/ ) I am having a lot of trouble getting anything beyond a simple Hello World program that outputs to the console using printf working.…
Hello,
I am working on a COFF file parser that will be used to help load our code on to our C6472 part. The data for each section is read in by reading the number of bytes (defined in the section header) from the file pointer offset in the file (also…
Hi Tanmay,
Kernel boot log (dmesg):
root@asp3:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.1.46-g999 (oe-user@oe-host) (aarch64-se3linux-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2…
Hi All,
I want to transfer data from a host PC to the EVM via PCIe, and have been using two settings during my investigations; the factory-original positions, and the positions given in the readme.pdf file for the PCIE Boot Example given in .\mcsdk_2_00_02_14…
Part Number: TMS320F28027 Tool/software: TI C/C++ Compiler Hii,
I am using this code for three phase voltage source inverter for generating spwm. Can you tell me which part of code affect modulation index or changing modulation index?
#include <stdio…
still no luck. I deleted the 6lbr directory and did a fresh clone, i.e.
git clone --recursive https://github.com/cetic/6lbr
git checkout ff69ae4214407eeec4c71f87589ac4bc7d3a8a49
make all plugins tools
make install
current log looks like this…