Part Number: TAS2120 Hello,
We have integrated the TAS2120 into our custom hardware. We are able to play audio succesfully from linux using aplay. Changing the volume level through alsamixer seems to work as expected while the audio stream is playing…
Part Number: TAS2120 Hello,
We are currently evaluating the TAS2120 using both the evaluation kit and our own custom hardware design.
Would it be possible to provide:
A generic/example configuration binary (.bin) for TAS2120 ( tas2120RCA1.bin…
Part Number: TAS2120 Hi,
I am currently working on a project using the TAS2120 audio amplifier, and my host microcontroller is the ESP32.
I plan to control the TAS2120 via I2C to configure the registers and stream audio. Could you please provide the…
Part Number: TAS2120 Hi technical team,
Can I use the TAS2120 without a battery? Specifically, can I power it with a 5V source instead of a battery?
Additionally, is there another part number (PN) recommended for a system without a battery? I am using…
Part Number: TAS2120 Hello,
For our application, we are interested in designing a smart audio amp paired with high inductance speaker drivers (0.3mH) and noticed that the TAS2120 datasheet recommends a max speaker inductance value of 100 uH, or 0.1mH…
Part Number: TAS2120 Is it possible (or advisable) to utilise the internal boost feature to power other devices. For example, as an audible alarm, we may want to sent short radio messages and operate illumination. While this could be achieved with a separate…
Part Number: TAS2120 Tool/software: Is there an update on this? Is this project still due for release and if so when will parts be available for test? The link to the EVM is also missing.
Part Number: TAS2120
When driving high-inductance actuators, the phase shift of current and voltage in the load can cause reverse-current issues triggering Class-D amplifier protection schemes such as over-current and over-voltage.
The attached spreadsheet…
Other Parts Discussed in Thread: TAS2120EVM , TAS2120 Tool/software: I downloaded TAS2x20 v3.00.targ.gz and installed on PPC3 v 3.2.1. when I launch the TAS2x20 application with the TAS2120EVM + AC-MB DC058 Rev C, I get this err message "Connected EVM…
Part Number: TAS2120 Tool/software: Datasheets Table 6-46 shows the I2C Mode Address Selection for TAS2120.
I think this a wrong table because there is no AD1 pin nor AD2 in this device.