Part Number: TAS2563 Hello, We are integrating a TAS2563 amplifier with an NXP i.MX RT1064 running Zephyr. Audio works correctly when the TAS2563 is configured in bypass/ROM mode, but the speaker remains silent when using a PPC3-generated DSP/Tuning …
Part Number: TAS2563 Hello.
We are using TAS2563 and trying to use the Dynamic EQ (DEQ) function configured in PurePath Console 3.
1. DEQ is not working with the PPC3-generated binary
We configured the DEQ parameters in PPC3 and generated a binary…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2770 Miele is reporting EMI issues with the TAS2563 device. See their translated E-mail and questions below.
Please support me in helping me to answer their questions and providing them valuable…
Part Number: TAS2563 Hello,
We have several questions regarding AMP_LEVEL and DVC_PCM on the TAS2563.
1. Recommended usage of AMP_LEVEL and DVC_PCM
According to the datasheet, VAMP = Input + ADVC + AAMP
Our current settings are: AMP_LEVEL = 16…
Part Number: TAS2563 Greetings,
I would like to configure the TAS2563 appropriately for various parameters like over-current,temperature, along with that would want the audio output to be optimized.As per the datasheet it suggests usage of PP3 software…
Part Number: TAS2563 I understand that voltage and current information can be output from the TAS2563 via TDM TX (SDOUT). Could you please clarify how the receiving side is expected to use this information?
Part Number: TAS2563 Hi TI Team,
I am using the TAS256x baremetal driver on a custom MCU. I exported PPC3 tuning files (a Snapshot with obvious EQ/Gain changes) and updated the CFG0_MUSIC_COEFF arrays in my C code.
The I2C writes execute perfectly…
Part Number: TAS2563 There are many registers that are mentioned in the datasheet description text but are not included in the register map.
For example the LIM_MAX_ATN, LIMB_TH_MAX, LIMB_TH_MIN, LIMB_INF_PT, DVC_RAMP, DVC_PCM registers.
Is there…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS5805M , TAS5805 Dear TI Engineer,
Can you help confirm if TAS2563 can support Echo Cancellation function? From the datasheet we can see that it has two SDOUT pin, and this pin can be used as…
Part Number: TAS2563 Hi,
We are using two TAS2563 IC interface spakers in our product.
I have belwo questions to understand more:
When our device is shutdown only VBAT power is present and VDD & IOVDD is off. In this case, the register configurations…