Part Number: TAS2563 Tool/software: Using the PurePath Console 3 to get config register values based on my speaker and project. The output of that is below. The example C code for how to write those registers via I2C is very confusing IMO and I would…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2562 , TAS2781 We are working with a system using the QCS8550 chipset and TAS2563 amplifier, connected as shown in the attached schematic. I2S has been used for audio data transfer and I2C for the…
Part Number: TAS2563 Hello!
As a follow-up to e2e.ti.com/.../tas2563-weak-echo-reference-signal-from-smart-amp , I can't find a definition of the "Audio Out" channel. Where is it taken from? Which blocks occur after it? Volume Control?
Thanks!
Part Number: TAS2563 Tool/software: Hello Expert,
Could you help us export .PPC3 file of TAS2563 with enable echo reference function and playback function. There is no PDM MIC used. For playbacl function, the sampling frequency is 16khz and boost voltage…
Part Number: TAS2563YBGEVM-DC Other Parts Discussed in Thread: TAS2563 We are using the TAS2563 BGA amplifier in a battery-powered product with a current budget of around 130 mA.
We observed that:
The amplifier consumes about 65 mA when playing…
Part Number: TAS2560EVM Other Parts Discussed in Thread: TAS2563 , TAS2560 HI We order TAS2560EVK but want to use TAS2563 in production. Doi i need to order TAS2563EVK, or will filtering and setting i make for TAS2560 work for TAS2563 Thansk Mikal
Part Number: TAS2563 Tool/software: Hi Sirs,
I would like to find the inductors (L2 and L3) for my system (with TAS2563) . However, I looked around and it seems there is no 0402 size that meets the 2A current specification. Could you please give me…
Part Number: TAS2563 Tool/software: to whom it may concern
I got the new TAS2563 EVM from TI. Thank you for your help!
However, I see that the jumper defaults on the new EVM are different from what we discussed last time (pictured below). What kind…
Part Number: TAS2563 Tool/software: 1. The two curves of Efficacy vs Output power and THD+N vs Output power in the TAS2563 datasheet are as follows: Please provide a curve chart of PVDD=5V. If not, can you provide the efficiency and THD+N of PVDD=5V at…