Part Number: TAS3251 Hi Team,
Currently, we have one product, is having the issue, please see if anybody can have some idea about this, thanks in advance.
" The power supply voltage is 36V. During mass production, there are around 10% units will burn…
Part Number: TAS3251 i have a question and i will be grateful if you can help me. main project: connecting STM32H743 to TAS3251 and playing an mp3 file saved on a usb flash which is connected to stm32. problem: cant get dsp to work. (tas3251 plays the…
Part Number: TAS3251 Hello,
in the current production run we have a higher number of TAS3251 that don't work properly and I'm looking for a clue what might be the problem and I'm seeking for advice if there is something I could further measure.
In…
Part Number: TAS3251 Hello,
We have a board with 4x TAS3251 with each Amp configured in BTL mode where one Amp doesn't output any audio sporadically after power-up. The interesting thing is that it can also be a different Amp at another time.
When…
Part Number: TAS3251 Thank you for your support. I have a question regarding how to achieve the highest audio performance with the TAS3251.
On page 23 of the datasheet, it states:
"In situations where the highest audio performance is required, bringing…
Part Number: TAS3251 Hello,
After reading the dedicated app note and carrefully watching the EVM layout, I still have some questions about the PFFB implementation.
Part Number: TAS3251 Hello,
We are running 96 kHz audio through the TAS3251 using the internal DSP (a small number of filters: low-pass, peaking, and all-pass).
As per the datasheet (96KhZ, R=128), the recommended clocking for 96 kHz operation (see…
Part Number: TAS3251 Hello,
we have designed a PCB using the TAS3251 and now it seems like the output is inverted in relation to the input.
Is it possible that the TAS3251 inverts the signal?
The only hint I could find in the datasheet is the 'inverting…
Part Number: TAS3251 Hello there,
We are building a system using TAS3251. Would you kindly review schematic with PFFB circuit and advise?
We have designed it using the PFFB application note and are fairly confident in the design.
Additionally…
Part Number: TAS3251 The datasheet for the TAS3251 contains a very superficial register map of the device. TI encourages engineers to use PPC3 for DSP design. However I would like to be able to have more direct control over the design process. Is there…