Part Number: TAS3251
Tool/software:
Hello,
on the TAS3251 outputs we have the following filter network and during our first tests all resistors of the Zobel network burned.
The speaker have an impedance of 6 Ohms.
I told the buying department…
Part Number: TAS3251-SW Other Parts Discussed in Thread: TAS3251 , Tool/software: 客服工程师你好!我电脑重装了系统,安装PurePath Console 3软件后,里面没有TAS3251的调音工具。这个是不是电脑重装系统后要重新申请 TAS3251-SW吗?
Part Number: TAS3251 Other Parts Discussed in Thread: TPA3223 , TPA3255 , TPA3251 , TAS5558 , TAS5828M , Tool/software: Dear expert:
For this product, the customer means that the power amplifier needs to support both fixed-resistance output (push two…
Part Number: TAS3251 We have designed a circuit using TI's TAS3251DKQR (HSSOP56) audio amplifier.
The configuration file is based on the PPC3 exported data.( T10 dsp v11.h )
Our system works normally in 4‑wire input mode . However, when configured…
Part Number: TAS3251 I have developed a board based on TAS3251. I'm trying to configure it to be I2S master (i.e. drive SCLK and LRCLK). The following is my configuration. I have only added the section between "I2S master begin" and "I2S master end".…
Part Number: TAS3251 Tool/software: Hi ti team,
A project uses 4PCS of TAS3251, each using different software, found that TAS3251 only has two addresses, may I ask how to set them?
Part Number: TAS3251 Tool/software: The swap registers mentioned in the datasheet seem to be different from those in the generated config file. Is the datasheet wrong? or Am I missing something.
Below is from the cfg file:
#swap command w 94 00…
Part Number: TAS3251 Tool/software: There is mention of the the "Level Meter" in the datasheet in sections 7.5.1 and 7.5.2.10 (screenshots attached)
Yet, I don't see the actual register addresses where I can:
read the level meter.
set…
Part Number: TAS3251 Tool/software: I'm looking at TAS3251 Process flows document . Process flow 5 and 6 have these register: Sub Mix ScratchL and Sub Mix ScratchR . What do they do?
Thanks,
Sia
Part Number: TAS3251 Other Parts Discussed in Thread: TPA3251 , OPA1632 , , TAS5756M Tool/software: TI Team, Input pin bias voltage:
What is the DC bias of the SPK_INA± on the TPA3251 device? Following the slaa702.pdf application note, we are implementing…