Part Number: TAS5441-Q1 Hello, we see following faults reported by TAS5441. Can you please confirm if this is expected results?
In all cases, speaker is not attached.
1st row: detected open load on SPKR+ and Over-current shutdown on SPKR- ? Shouldn…
Part Number: TAS5441-Q1
Hi,
there no detail on when the repetition check phase works during diagnosis in the TAS5441-Q1
What is the exact capacitance threshold that triggers the diagnostic check phase repetition (up to 5 times) in TAS5441-Q1? Is…
Part Number: TAS5441-Q1 Tool/software: Hello,
First row of Table 7-4 shows Data bits [D2 D1 D0] = [0 0 0] to set the Switching Frequency to 400kHz whereas on second row, when D0 = "1" , the Switching Frequency is set to 500kHz.
I think only D0 is…
Part Number: TAS5441-Q1 TAS5441LQPWPRQ - Please provide the driver for this model, along with detailed relevant information and application instructions. Thank you
Part Number: TAS5441-Q1 Hello team we choose TAS5441-Q1 amplifier IC in our design.
1) Please suggest power supply IC for amplifier(please consider audio noise point of view), the output of amplifier is 20W and 10W.
2) What is peak power and nominal…
Part Number: TAS5441-Q1 Dear Team,
I am working on TAS5441-Q1 IC, this IC I used in one board circuit.
On single board I have used three IC's. one IC is for differential output, another two ICs are for single-ended outputs.
When I am connecting…
Part Number: TAS5441-Q1 Hi expert,
What is the input audio to output sound delay for tas5441-q1?
This delay data will affect the effectiveness of our noise reduction algorithm, so we now need to collect this delay data.
Thanks
Xiaoxiang
Part Number: TAS5441-Q1
Dear team,
I kindly request you to please let us know the functionality about FAULT Pin-TAS5441-Q1.
Now, I am working on Class D amplifier IC-TAS5441-Q1, initially IC is working properly. when I was testing this IC in play…
Part Number: TAS5441-Q1 Tool/software:
Hi,
The audio amplifier Part No : TAS5441QPWPRQ1 selected in our design to drive the external speaker of 4 OHM, 10Watt.
The device is operating at 15V DC (PVDD) to drive the external speaker.
Does this chip…
Part Number: TAS5441-Q1 Other Parts Discussed in Thread: TPA3111D1-Q1 , TPA3112D1-Q1 Tool/software: Hello,
My customer is asking about load dump in TAS5441-Q1.
Are TPA3111D1-Q1 or TPA3112D1-Q1 load dump function?
Also, are there any other in-vehicle…