Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 , TAS5717 , TAS5717EVM Hello TI team.
I'm developing an application using the TAS5731M. I'm having trouble communicating with the TAS5731MEVM. I followed slou331a's instructions: Changing…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5713 , TAS5825M , TAS5822M , TAS5805M
Hello. I'm trying to configure the TAS5731M Amplifier, but I can only initialize it, but nothing sounds. It goes from 0mA to 45mA when I start it, but I…
Part Number: TAS5731M Digital I2S signal is present
Audio sampling rate Fs: 44.1 kHz
MCLK: 256 x Fs
TAS5731M I2C is working. I write I2C to the following registers as below
1. REG 0x07 = 0x00 (Master volume 24 dB)
2. REG 0x08 = 0x00 (Channel…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 After sending 7 bit 0x36 + 1 bit Read, TAS5731M is not giving me ACK. How can I diagnose the problem. Any diagnostic procedure to check the health of TAS5731M?
CH0 - SDL
CH1 – SDA
…
Part Number: TAS5731M Tool/software: When our TV does not play any audio, the speaker will have some background noise. Does TAS5731M have a similar noise gate function to eliminate such background noise?
Part Number: TAS5731M Tool/software: Regarding the power-on timing of the 5731, 1. At present, our AVDD/DVDD(the two power supplies use the same) will be later than PVDD, but we can ensure that the two power supplies are stable, and then pull up PD and…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 Tool/software: Hi: I have a question about the power-down sequence of TAS5731 that I need to consult. The specification requires “Ramp down AVDD/DVDD while ensuring that it remains above 3…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 The Bluetooth module transmits audio data to the TAS5731M using the I2S bus. The current hardware test results show that the volume adjustment is non-linear, when the volume key progress bar…
Part Number: TAS5731M Tool/software: We have a Bluetooth hardware board which includes the TI audio chip TAS5731M, the board connected with mobile phone by Bluetooth A2DP connection. When the mobile phone is playing the music, mobile phone will send the…
Part Number: TAS5731M Other Parts Discussed in Thread: PCM9211 , , PCM5102A , PCM2706 I have a custom PCB with the same schematic of the EVM board. I'm trying to initialize the chip, I have a workling i2c communication. But I cannot get any sound from…