Part Number: TAS5806M Hi,
Because of our customer can't download the PPC3 and can you help to provide one default firmware to customer to test the function firstly? thanks.
Part Number: TAS5806M Other Parts Discussed in Thread: TAS5822M I have PPC3 installed but I cannot find a download link or even a request to download link anywhere on the ti.com site for the TAS5806M PPC3 app. Please advise how to get the PPC3 app for…
Part Number: TAS5806M Other Parts Discussed in Thread: TAS5805M Hi Expert.
My customers want to know do we have demo code for driving the TAS5806M under Linux platform.
Besides, are the driving code (mainly the process of writing and reading of registers…
Part Number: TAS5806M Other Parts Discussed in Thread: TAS2110 , TAS2563 , Tool/software: Hi team,
Does TAS5806D support low latency interpolation filters? It is not mentioned in the datasheet but a checkbox for the feature is available on PPC.
If…
Part Number: TAS5806M Tool/software: I'm using TAS5806m IC for making a amplifier board. My Speaker is 4ohms and I'm using this in stereo and the mcu is ESP32. My configuration is BD Modulation. I'm getting I2C address and following the below process…
Part Number: TAS5806M
Tool/software:
Applying the 24V supply to PVDD in that case TAS5806MDCPR amplifier is heating. how to overcome or reduce this heating of amplifier. using below schematic in that C29, C32 used 22uF/50V and C30, C31 using the 0…
Part Number: TAS5806M Hi, TI Support Team
The following inquiries have been received from customers.
It is related to heatsink application of TAS5806M product.
It is planned to design under the following conditions, but do I need to apply Heatsink…
Part Number: TAS5806M Other Parts Discussed in Thread: PCM1808EVM , PCM1808 Hi,
I correctly configured the esp32 to receive audio via bluetooth and transmit it to the TAS5806M with sample_rate 44100 and bits_per_sample 16 and everything works correctly…
Part Number: TAS5806M Hello everyone,
We are currently experiencing overcurrent troubles with the TAS5806M used in mono mode (PBTL) with a 4Ohm speaker.
We had already used this component successfully with an earlier proto board, where we were able…
Part Number: TAS5806M Hi,
I would like to transmit the digital audio output from the SDOUT pin of the TAS5806M to 100 DACs simultaneously without having any signal loss.
What transmission method would you recommend?